FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Wiring length
FAQ
Wiring length
In the Instruction Manual of the FR-A700, it is described that the wiring length between INV and IM should be 100 m or less under Vector control. How about under Real sensorless vector control?
- Category :
Answer
Under Real sensorless vector control, the maximum wiring length is 500 m. Under Vector control with encoder, the maximum wiring length is 100 m.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700