Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21136
  • Release Date : 2018/08/22 16:26
  • Print

Motor: SF-HJCA

Answer

Configure the same setting as the SF-HRCA. Configure the same setting as the SF-HRCA. A700, E700, D700, F700PJ: Pr.71 = 50F700P, F700: Pr.71 = 1 (Reference) SF-HRCA: steel plate frame, SF-HJCA: casting frame (The electrical characteristics are the same.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?