Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21141
  • Release Date : 2018/08/22 16:26
  • Print

FR Configurator

How can I transfer the parameter of the 500 series that has been backed up (.mel file) with inverter set up software SW1 to 700 series? I also have FR Configurator SW3.
Category : 

Answer

Save the parameter file (.rpm) after reading the system file (.mel) created in SW1. With the saved parameter file (.rpm), the parameter of the 700 series can be created and written to E720 by using the convert function of SW3. For the convert function, refer to "4.7 Convert (System Area)" in the Instruction Manual of SW3.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries