Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21143
  • Release Date : 2018/08/22 16:26
  • Print

FR-RC

Answer

Pr.30 = "1" and Pr.70 = "0".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-D700, FR-E700, FR-F700, FR-F700P, FR-F700PJ
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?