FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Vector control
FAQ
Vector control
I am planning to perform Vector control with the FR-A700 and SF-V5RU together. For the wiring with the thermal protector, a resistor of 2 W 1 k? is installed. When using the external power supply with the sink logic, where should be the resistor installed?
- Category :
Answer
Install the resistor between the terminals PC and OH.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700