Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21174
  • Release Date : 2018/08/22 16:26
  • Print

FR Configurator SW3 (CC-Link Seamless)

Why is "Error: 0X80010016" displayed when Pr.77 (Parameter write selection) and Pr.79 (Operation mode selection) are written via CC-Link communication.
Category : 

Answer

Pr.77 and 79 cannot be changed via CC-Link communication.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
Others
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?