FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Watt-hour meter clear and operation hour meter clear
FAQ
Watt-hour meter clear and operation hour meter clear
Why is the value out of the setting range read when reading Pr.170 (Watt-hour meter clear) and Pr.171 (Operation hour meter clear)?
- Category :
Answer
The values are set to Pr.170 and 171 when the monitor value of cumulative power and actual operation time overflows. It does not affect the operation. Use it as it is.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700