FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Writing set frequency by CC-Link communication
FAQ
Writing set frequency by CC-Link communication
When a value more than the upper limit frequency is written to RWwn+1 (set frequency), will an error occur?
- Category :
Answer
No error will occur because up to 400 Hz that is the upper limit of the setting range can be written.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700