FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Remote register when instruction code execution request is issued at CC-Link communication
FAQ
Remote register when instruction code execution request is issued at CC-Link communication
When the instruction code execution bit is turned ON with other than the data read (such as parameter write), what happens to the value of the RWrn+3 read data?
- Category :
Answer
The value "0" is stored.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700