FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > 4 to 20 mA output
FAQ
4 to 20 mA output
Is the current signal output (4 to 20 mA) available?
- Category :
Answer
Yes. It is available by using the FR-A7AY (plug-in option). By setting Pr.307 (Setting for zero analog output) to "20" and Pr.309 (Analog output signal voltage/current switchover) to "10", 4 to 20 mA output is enabled.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700