FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Replacement
FAQ
Replacement
I have been performing CC-Link operation with the FR-A500. Which parameter should I pay attention to when replacing to the FR-A700?
- Category :
Answer
The station number and baud rate were set using the dial for the FR-A5NC, but parameter is used for the FR-A7NC. Pr.542 (Communication station number (CC-Link)) Pr.543 (Baud rate selection (CC-Link)) Refer to the document for the replacement of the FR-A500 with FR-A700. It can be downloaded at Mitsubishi Electric FA Global Website. Select FA HOME > Inverters FREQROL > Discontinued model, and download the renewal document BCN-C21002-087 in the FREQROL-A500(L) field.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700