FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > DC reactor
FAQ
DC reactor
In the list of options on the catalog of the FR-A700 (F700P), DC reactors (FR-HEL) are described up to 55K. Is the 75K or higher DC reactor available?
- Category :
Answer
The 75K or higher DC reactor is included in the 75K or higher inverter. The option cannot be purchased separately.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700