Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21266
  • Release Date : 2018/08/22 16:26
  • Print

Frequency setting signal

While the current is input from the terminal 4, the FWD blinks and operation does not start even though the AU terminal is ON. Pr.267 (Terminal 4 input selection) is set to "0" and voltage/current input selection switch of terminal 4 is turned ON ("I" for E700 and D700). What are the possible causes for this?
Category : 

Answer

Check that the wiring of the terminal 4 and 5 are not reversed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?