FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Frequency setting signal
FAQ
Frequency setting signal
While the current is input from the terminal 4, the FWD blinks and operation does not start even though the AU terminal is ON. Pr.267 (Terminal 4 input selection) is set to "0" and voltage/current input selection switch of terminal 4 is turned ON ("I" for E700 and D700). What are the possible causes for this?
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
Check that the wiring of the terminal 4 and 5 are not reversed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700