FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Rated frequency setting
FAQ
Rated frequency setting
When the spindle motor with 200 Hz rated frequency is used, "OL" (overload) is displayed at 4 to 5 Hz and the speed does not increase.
How should I configure the setting?
How should I configure the setting?
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
Check that Pr.3 (Base frequency) is set to "200 Hz".
Adjust Pr.0 (Torque boost) as necessary.
Adjust Pr.0 (Torque boost) as necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700