FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Life diagnosis
FAQ
Life diagnosis
In the life check function for the main circuit capacitor, how is the life diagnosis performed?
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
When Pr.259 (Main circuit capacitor life measuring) is set to "1", the life diagnosis is ready.
Turning OFF the power supply starts measuring the life of the capacitor.
The life is determined according to the decreasing rate and time.
Turning OFF the power supply starts measuring the life of the capacitor.
The life is determined according to the decreasing rate and time.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700