FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Electronic thermal O/L relay
FAQ
Electronic thermal O/L relay
When the motor with 0.2 kW is used, trips occur frequently due to the electronic thermal O/L relay error.
Can I set the operation time of the electronic thermal O/L relay?
Can I set the operation time of the electronic thermal O/L relay?
- Category :
Answer
Check that the correct rated motor current is set in Pr.9 (Electronic thermal O/L relay).
No parameter is available for setting the operation time of the electronic thermal O/L relay.
No parameter is available for setting the operation time of the electronic thermal O/L relay.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700