FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > FR-PA07
FAQ
FR-PA07
Is the FR-E5P (back cover and adapter) provided with the FR-E500 necessary for the option FR-PA07?
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
Since the FR-PA07 has the back cover and adapter, the FR-E5P is not necessary.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700