Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21306
  • Release Date : 2018/08/22 16:26
  • Print

Parameter copy of FR-Configurator

Can I save the parameter and copy it to three inverters at the same time with FR-Configurator (FR-SW3-SETUP-WJ)?
Category : 

Answer

The parameter can be copied to only one inverter.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?