FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Parameter copy method of FR-Configurator
FAQ
Parameter copy method of FR-Configurator
Can I read the set inverter parameter and copy the data to other parameter with FR-Configurator (FR-SW3-SETUP-WJ)?
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
The data can be copied to other inverters.
1. Save the parameter of the inverter to be copied with extension "pr3" by using "export".
2. Replace the connected inverter with the target inverter.
3. Startup the software and establish the communication with the inverter.
4. Click the parameter list and open the file that was saved by "import". At this time, "present value" or "setting value" can be selected. Select "setting value" to reflect the parameter to be copied to the setting value field in the parameter list.
1. Save the parameter of the inverter to be copied with extension "pr3" by using "export".
2. Replace the connected inverter with the target inverter.
3. Startup the software and establish the communication with the inverter.
4. Click the parameter list and open the file that was saved by "import". At this time, "present value" or "setting value" can be selected. Select "setting value" to reflect the parameter to be copied to the setting value field in the parameter list.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700