Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21314
  • Release Date : 2018/08/22 16:26
  • Print

Supported model for FR-Configurator

Answer

The FR-E700 is not supported by FR-SW2-SETUP-WJ.
The FR-E700 series are supported by FR-SW3-SETUP-WJ.
This software can be downloaded from the Mitsubishi Electric FA Global Website.
If you have FR-SW2-SETUP-WJ, it can be updated.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?