FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Capacity selection
FAQ
Capacity selection
How can I select the inverter capacity when using a motor?
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
Select the inverter capacity so that the rated output current of inverter ? rated motor current × 1.1.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700