Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21330
  • Release Date : 2018/08/22 16:27
  • Print

Brake resistor

I do not have the high-duty brake resistor FR-ABR-1.5K (inverter option). Which brake resistor should I use for the inverter with capacity of 1.5K?
Category : 

Answer

Use high-duty brake resistor FR-ABR-2.2K. (Shared with the 1.5K inverter.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?