FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Output frequency
FAQ
Output frequency
What is the upper limit of the inverter output frequency (Hz) in the initial setting?
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
In the initial setting, it is set to 120 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700