FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Frequency setting
FAQ
Frequency setting
I want to change the output frequency using CC-Link. Is it changed by changing the setting of Pr.1 (Maximum frequency)?
- Category :
Answer
Even though the maximum frequency setting is changed using CC-Link, the running frequency is not changed.
By writing the set frequency to the remote register RWw1 and turning ON RYD or RYE, the frequency setting completion turns ON and the frequency is set. (Set the frequency in units of 0.01 Hz.)
By writing the set frequency to the remote register RWw1 and turning ON RYD or RYE, the frequency setting completion turns ON and the frequency is set. (Set the frequency in units of 0.01 Hz.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700