FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Easy setting mode
FAQ
Easy setting mode
When I tried to change Pr.79 (Operation mode selection) in the easy setting mode to input the start command and frequency command on the operation panel, "HOLD" was displayed.
How can I clear it?
How can I clear it?
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
If "HOLD" is displayed, the key lock mode enabled.
Press the "MODE" key for two seconds.
Then, change the setting of Pr.79 to "1".
Press the "MODE" key for two seconds.
Then, change the setting of Pr.79 to "1".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700