Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21352
  • Release Date : 2018/08/22 16:27
  • Print

Offline auto tuning

When offline auto tuning completes, the setting value of Pr.96 (Auto tuning setting/status) becomes "3". Should I change this setting when performing the actual operation?
Category : 

Answer

Leave the setting of Pr.96 as "3".

It indicates that auto tuning has been completed and the motor constant has been read.

When it is changed unnecessarily, the constant of auto tuning will not be used.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?