FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Operation mode setting
FAQ
Operation mode setting
When Pr.79 (Operation mode selection) of the inverter is set to "3", operation is not changed by changing the setting of Pr.275 (Stop-on contact excitation current low-speed multiplying factor). What are the possible causes?
- Category :
Answer
The stop-on-contact control does not function in the combined operation mode.
Perform the control in the External operation mode.
Perform the control in the External operation mode.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700