FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > PU operation
FAQ
PU operation
1. Can I input the emergency stop during the PU operation?
2. Can I reverse the input of the emergency stop?
3. Will the operation continue when the operation is stopped by turning ON the emergency stop, and then turned OFF the emergency stop again?
2. Can I reverse the input of the emergency stop?
3. Will the operation continue when the operation is stopped by turning ON the emergency stop, and then turned OFF the emergency stop again?
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
1. Yes.
2. Set Pr.17 to "2".
3. If the start signal is ON, the operation continues even the emergency stop is OFF.
2. Set Pr.17 to "2".
3. If the start signal is ON, the operation continues even the emergency stop is OFF.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700