FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > FR-PA07
FAQ
FR-PA07
How can I disable the dial operation except the frequency setting when using the enclosure surface operation panel FR-PA07?
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
Operations cannot be enabled separately.
You only can disable or enable all the operations.
You only can disable or enable all the operations.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700