FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Monitor
FAQ
Monitor
Which current and voltage of the phase (maximum value, average value, etc.) are displayed on the operation panel monitor?
Down to two decimal point is displayed for the current. How accurate is this value?
Down to two decimal point is displayed for the current. How accurate is this value?
- Category :
Answer
The output current monitor of the inverter displays the output current effective value of the three phases measured by the current sensor.
It does not display the current value of the specific phase.
The output voltage monitor displays the output voltage target value (effective value) of the inverter, and it is not the actual measured value.
For the second digit after the decimal displayed on the output current monitor of the inverter, the accuracy is approximately 90 %.
It does not display the current value of the specific phase.
The output voltage monitor displays the output voltage target value (effective value) of the inverter, and it is not the actual measured value.
For the second digit after the decimal displayed on the output current monitor of the inverter, the accuracy is approximately 90 %.
- Product Name
- Inverter, magnet motor drive
- Series
- FR-E500