Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21409
  • Release Date : 2018/08/22 16:27
  • Print

Automatic overload control of inverter

Do you provide an inverter that can detect the load current of the motor and automatically controls the frequency so that the motor may not overloaded?
Category : 

Answer

The inverter has the current limit function.
This automatically controls the frequency so that the preset current value may not be exceeded.
(Note that the motor load is always determined by the mechanical load. If the overload condition persists, you need to mitigate the mechanical load.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-S500, FR-E500, FR-F500, FR-A500
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?