FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Automatic overload control of inverter
FAQ
Automatic overload control of inverter
Do you provide an inverter that can detect the load current of the motor and automatically controls the frequency so that the motor may not overloaded?
- Category :
Answer
The inverter has the current limit function.
This automatically controls the frequency so that the preset current value may not be exceeded.
(Note that the motor load is always determined by the mechanical load. If the overload condition persists, you need to mitigate the mechanical load.)
This automatically controls the frequency so that the preset current value may not be exceeded.
(Note that the motor load is always determined by the mechanical load. If the overload condition persists, you need to mitigate the mechanical load.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-S500, FR-E500, FR-F500, FR-A500