Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21422
  • Release Date : 2018/08/22 16:27
  • Print

Encoder feedback speed accuracy

How high is the accuracy for the inverter command output when using encoder feedback control and vector control of the FR-A5AP (FR-A520)?
Category : 

Answer

The speed variation rate is as follows:
 - Encoder feedback control: ±0.2% - Vector control: ±0.02% (mentioned in FR-A5AP Instruction Manual)
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
FR-A500
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?