FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Output current detection
FAQ
Output current detection
I am planning to choose the FR-A240E.
I want to detect the state where the actual output current higher than the set value flows to detect motor signal loss, and input the detection signal to the programmable controller.
Can I do this with the FR-A240E?
I want to detect the state where the actual output current higher than the set value flows to detect motor signal loss, and input the detection signal to the programmable controller.
Can I do this with the FR-A240E?
- Category :
Answer
The FR-A500 series that is the successor of the FR-A200E series has a function similar to output current detection of the FR-E500.
Consider using the FR-A500 series.
Consider using the FR-A500 series.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200, FR-A500