FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Items controllable via CC-Link
FAQ
Items controllable via CC-Link
I use an inverter and multiple servo amplifiers in a single system.
Can I control the following items by using CC-Link?
1. Can I control items controlled via the external terminals via CC-Link?
2. I want to monitor the current value and output frequency and change the command frequency arbitrarily during operation. Is this possible?
Can I control the following items by using CC-Link?
1. Can I control items controlled via the external terminals via CC-Link?
2. I want to monitor the current value and output frequency and change the command frequency arbitrarily during operation. Is this possible?
- Category :
Answer
1. Not all items can be controlled.
- Functions that cannot be controlled JOG, AU, CS, OH, X10, X11, X12, and X16 functions (Other functions can be controlled.)
- Terminals that allow for ON/OFF input via CC-Link STF, STR, RH, RM, RL, JOG, RT, AU, CS, and MRS (Functions of RH, RM, RL, JOG, RT, AU, and CS can be changed by Pr.180 to 186. JOG, AU, and CS can be turned ON/OFF via CC-Link, but the functions assigned to these terminals do not work.) JOG, AU, and CS can be turned ON/OFF via CC-Link, but the functions assigned to these terminals do not work.)
2. Yes.
- Functions that cannot be controlled JOG, AU, CS, OH, X10, X11, X12, and X16 functions (Other functions can be controlled.)
- Terminals that allow for ON/OFF input via CC-Link STF, STR, RH, RM, RL, JOG, RT, AU, CS, and MRS (Functions of RH, RM, RL, JOG, RT, AU, and CS can be changed by Pr.180 to 186. JOG, AU, and CS can be turned ON/OFF via CC-Link, but the functions assigned to these terminals do not work.) JOG, AU, and CS can be turned ON/OFF via CC-Link, but the functions assigned to these terminals do not work.)
2. Yes.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500, FR-A500