Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21471
  • Release Date : 2018/08/22 16:27
  • Print

Inverter operation against power supply voltage drop

If the power supply voltage drops to 60% to 70% level in approximately 50 to 100 ms, how does the inverter (A500) operate?
Category : 

Answer

Depending on the load current, undervoltage protection (UVT) or instantaneous power failure protection (IPF) is triggered to shut off the inverter output, and the (inverter) trips. (Reset the inverter to restart it.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries