FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameters not covered in manual are displayed
FAQ
Parameters not covered in manual are displayed
On the FR-E520-0.4K, 0.75K, and 2.2K inverters, No.168 and No.169 that are not covered in the manual are displayed.
Pr.168 is set to "7362" and Pr.169 is set to "5". What are these parameters?
Pr.168 is set to "7362" and Pr.169 is set to "5". What are these parameters?
- Category :
Answer
Pr.168 indicates the inverter software version.
Pr.169 indicates the inverter software subversion history.
These two parameters are only used by the manufacturer to determine the software version.
Therefore, there are read-only and cannot be changed.
Pr.169 indicates the inverter software subversion history.
These two parameters are only used by the manufacturer to determine the software version.
Therefore, there are read-only and cannot be changed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500