Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21585
  • Release Date : 2018/08/22 16:28
  • Print

Difference from conventional product (parameter unit)

Should I use the parameter unit with the conventional inverters to change the parameters?
Category : 

Answer

The parameter unit is not available.
Use two internal potentiometers to set the electronic thermal O/L relay and acceleration/deceleration time, and two switches to set the maximum frequency.
Product Name
Inverter, magnet motor drive
Product Category
Inverter speed controller
Series
SC-A
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?