FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Plug-in Options > Compatibility of plug-in option
FAQ
Compatibility of plug-in option
Can I use the plug-in option used with the FR-A100 with the FR-A100EXCELLENT?
- Category :
Answer
Use the plug-in option dedicated for the FR-A100EXCELLENT.
To avoid an incorrect installation, the connector position for the plug-in option and the FR-A100EXCELLENT is different from the one for the FR-A100 plug-in option.
Do not install an incorrect option forcibly because doing so breaks the plug-in option unit.
The functions of the FR-EPB to FR-EPE are the same as those of the conventional FR-APB to FR-APE options.
For the FR-A100EXCELLENT, the FR-EPG and FR-EPH options are added.
To avoid an incorrect installation, the connector position for the plug-in option and the FR-A100EXCELLENT is different from the one for the FR-A100 plug-in option.
Do not install an incorrect option forcibly because doing so breaks the plug-in option unit.
The functions of the FR-EPB to FR-EPE are the same as those of the conventional FR-APB to FR-APE options.
For the FR-A100EXCELLENT, the FR-EPG and FR-EPH options are added.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- FR-A100