FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > What functions are added compared with FR-A200?
FAQ
What functions are added compared with FR-A200?
What functions are added to the FR-A200EXCELLENT compared with the FR-A200?
- Category :
Answer
The following functions are added or improved:
- Auto tuning function- Fast-response current limit operation is improved.- Characteristics of magnetic flux vector control is improved.- The carrier frequency setting range is extended.- Communication speed of plug-in option is improved.And others.
- Auto tuning function- Fast-response current limit operation is improved.- Characteristics of magnetic flux vector control is improved.- The carrier frequency setting range is extended.- Communication speed of plug-in option is improved.And others.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A200