FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-BU2
FAQ
FR-BU2
Can I use the brake unit FR-BU2 with the FR-E740-1.5K?
The motor capacity is 1.5 kW.
The motor capacity is 1.5 kW.
- Category :
Answer
You cannot use the brake unit FR-BU2 with the FR-E740-1.5K.
To use the brake unit, increase the inverter capacity to 2.2K.
You can use the brake unit with the FR-BU2-H7.5K and six discharging resistors GRZG200-10Ω connected in series.
To use the brake unit, increase the inverter capacity to 2.2K.
You can use the brake unit with the FR-BU2-H7.5K and six discharging resistors GRZG200-10Ω connected in series.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700