FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Terminal FM
FAQ
Terminal FM
Can I connect a DC ammeter with the internal resistance 160 Ω to the inverter terminal FM?
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
You can connect a 1 mA full scale ammeter with internal resistance 300 Ω or lower.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700