FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Switching between external operation and NET operation
FAQ
Switching between external operation and NET operation
To switch external operation and NET operation, I set Pr.181 (Terminal RM function selection) to "66", Pr.79 (Operation mode) to "0", and Pr.340 (Communication startup mode selection) to "1". Can I write frequency setting?
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
You can write frequency setting by setting Pr.339 (Communication speed command source) to "0".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700