FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Switching between external operation and NET operation
FAQ
Switching between external operation and NET operation
To switch external operation and NET operation, I set Pr.181 (Terminal RM function selection) to "66", Pr.79 (Operation mode) to "0", and Pr.340 (Communication startup mode selection) to "1". Is this setting correct?
Also, can I command output stop of the terminal MRS via communication?
Also, can I command output stop of the terminal MRS via communication?
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
You can switch between external operation and NET operation by turning ON/OFF the terminal X66 (RM).
You can switch while Pr.79 (Operation mode) is set to "6" (Switchover mode).
You can command output stop of the terminal MRS via communication by setting Pr.338 (Communication command source) to "0".
You can switch while Pr.79 (Operation mode) is set to "6" (Switchover mode).
You can command output stop of the terminal MRS via communication by setting Pr.338 (Communication command source) to "0".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700