Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21695
  • Release Date : 2018/08/22 16:28
  • Print

PU operation

Pressing the PU/EXT button does not switch to PU. I want to change the frequency.
An external start command is used and the frequency is set with the setting dial.
PU, EXT, and MON turn ON.
Category : 

Answer

If Pr.79 = 3, PU and EXT turn ON. Switching between PU and EXT is not available. Turn the setting dial to set the frequency and press the SET key to accept it.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries