FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > FR-DU07
FAQ
FR-DU07
Can I use the operation panel FR-DU07 used with the FR-A700 with the FR-E700?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > Others
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
Not possible.
Instead of FR-DU07, use FR-PA07 (or FR-PU07) as an operation panel for FR-E700.
Instead of FR-DU07, use FR-PA07 (or FR-PU07) as an operation panel for FR-E700.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700, and others