FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A7AR E kit (Relay output function)
FAQ
FR-A7AR E kit (Relay output function)
When using the optional FR-A7AR (Relay output function), can I set all of the three relay contacts to fault contacts?
- Category :
Answer
Yes, you can set all of the three relay contacts to fault contacts.
Set Pr.320 (RA1 output selection), 321 (RA2 output selection), and 322 (RA3 output selection) to "99".
Set Pr.320 (RA1 output selection), 321 (RA2 output selection), and 322 (RA3 output selection) to "99".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700