FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Parameter setting
FAQ
Parameter setting
After clearing all parameters, I used the setting dial in the PU operation mode and pressed the SET key at 60 Hz. "60.00" and "F" alternately flickered alternately and I set the frequency to 60 Hz.
Then, I set Pr.2 (Minimum frequency) to "10 Hz", but the inverter did not operate.
The RUN LED blinks rapidly. What happened?
Then, I set Pr.2 (Minimum frequency) to "10 Hz", but the inverter did not operate.
The RUN LED blinks rapidly. What happened?
- Category :
Answer
Check if Pr.13 (Starting frequency) is set to higher than 10 Hz.
Also check if a signal is input through the terminal MRS.
Also check if a signal is input through the terminal MRS.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ