FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Frequency setting
FAQ
Frequency setting
I perform remote operation by setting Pr.59 (remote function selection). When the acceleration signal (RH) is turned ON, the frequency rises. Is this frequency stored in any parameter?
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
It is not stored in a parameter but memorized as the frequency setting value after acceleration by the acceleration signal.
You can also choose whether or not to clear this frequency setting value when the power is turned off.
You can also choose whether or not to clear this frequency setting value when the power is turned off.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700